990-5995E-004

Skærmens menutræ

  • Status

    • Input (Indgang)

    • Output (Udgang)

    • Battery (Batteri)

    • Bypass

    • Status information (Statusinformation)

  • Alarm

    • Active alarms (Aktive alarmer)

    • Enable buzzer/Disable buzzer (Aktivér lydsignal/deaktiver lydsignal)

    • Log

  • Settings (Indstillinger)

    • General settings (Generelle indstillinger)

      • Language settings (Sprogindstillinger)

      • Display settings (Displayindstillinger)

      • Network (Netværk)

      • Password settings (Adgangskodeindstillinger)

      • Date and time (Dato og tid)

      • UPS information (UPS-information)

    • Advanced settings (Avancerede indstillinger)

      • System settings (Systemindstillinger)

      • Output settings (Udgangsindstillinger)

      • Bypass settings (Bypass-indstillinger)

      • Parallel settings (Parallelle indstillinger)

      • Battery settings (Batteriindstillinger)

      • Contacts and relays (Kontakter og relæer)

  • Service

    • Battery self-test (Batteriselvtest)

    • Export data to USB (Eksporter data til USB)

    • Display calibration (Kalibrering af display)

    • LCM settings (LCM-indstillinger)

  • Control (Kontrol)

    • Inverter ON/OFF (Vekselretter TIL/FRA)

    • Clear alarm(s) (Slet alarm(er))

    • Self-test (Selvtest)

  • About (Om)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.