SNMP
Description
The
page allows you to set the Simple Network Management Protocol (SNMP) settings.The EIFE interface supports SNMP, allowing a network administrator to access remotely an EIFE interface with an SNMP manager and to view the networking status and diagnostics of the EIFE interface in the MIBII format.
The users with Installer or Engineer role can change the SNMP settings.
Navigation to the SNMP Page
To view the
page, click .SNMPV1 Agent Settings
Setting |
Description |
Value |
---|---|---|
|
Allows you to enable or disable the SNMP agent. |
– |
|
Allows you to enter listening port number at which the SNMP agent listens for network traffic. |
|
|
Allows you to enter notification port number. |
|
System Objects Settings
Setting |
Description |
---|---|
|
Allows you to enter system location. |
|
Allows you to enter system contact person name. |
|
Allows you to select the System Name configuration mode:
|
|
Allows you to enter the system name manually. |
Community Names Settings
Setting |
Description |
---|---|
|
Allows you to enter get community name. |
|
Allows you to enter set community name. |
|
Allows you to enter trap community name. |
Enabled Traps Settings
allows you to select any of the following traps, which are disabled by default:
Setting |
Description |
---|---|
|
Generates a trap when the EIFE interface is powered ON. |
|
Generates a trap when SNMP is enabled. |
|
Generates a trap when an Ethernet port communication link is disconnected. |
|
Generates a trap when an Ethernet port communication link is reconnected. |
|
Generates a trap when an SNMP manager is accessing the EIFE interface with incorrect authentication. |
SNMP Managers Settings
Setting |
Description |
---|---|
|
Allows you to enter name or IP address of SNMP manager one. |
|
Allows you to enter name or IP address of SNMP manager two. |