Time Zone
Time Zone Configuration
Step |
Action |
---|---|
1 |
From the IFE menu bar, click . |
2 |
From the menu, in the submenu, click . |
3 |
In webpage, select the time zone of your region from the list. |
4 |
Select the check box if you have to set the daylight saving time. |
5 |
Select the beginning and end time of daylight saving from the and the list. |
6 |
Click to save the settings. |
Real Time Clock
The IFE server has a real time clock (RTC) to maintain date and time during power outage. The expected life time of the RTC is 15 years when operated at intermediate mode (in this mode, the battery is operated continuously for 4 days with an interval of 45 times over a period of 10 years).
The IFE server must maintain a crystal tolerance of ±20 ppm (typical)/±150 ppm (maximum) during the period of 15 years at -25 °C (-13 °F) to 85 °C (185 °F). The time drift by RTC chip varies from -16 s/day to +2 s/day. During power recycle, the RTC is able to maintain the date and time settings.