NHA2778902-13

Alarm setup overview

You can use ION Setup to configure unary, digital or standard (1-Sec) alarms.

If you make changes to the basic meter setup, all alarms are disabled to prevent undesired alarm operation.

NOTICE
unintended equipment operation
  • Verify all alarm settings are correct and make adjustments as necessary.
  • Re-enable all configured alarms.
Failure to follow these instructions can result in incorrect alarm functions.

Built-in error-checking

ION Setup dynamically checks incorrect setup combinations. When you enable an alarm, you must set up the pickup and dropout limits to acceptable values first in order to exit the setup screen.

**does this only apply to certain types of alarms?

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.