NHA2778902-13

Power factor min/max convention

The meter uses a specific convention for determining the power factor minimum and maximum values.

  • For negative PF readings, the minimum PF value is the measurement closest to -0 for PF readings between -0 to -1. For positive PF readings, the minimum PF value is the measurement closest to +1 for PF readings between +1 to +0.

  • For negative PF readings, the maximum PF value is the measurement closest to -1 for PF readings between -0 to -1. For positive PF readings, the maximum PF value is the measurement closest to +0 for PF readings between +1 to +0.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.