NHA2778902-13

Active tariff control mode

The active tariff is controlled based on the tariff mode.

  • When the meter is set to command mode, the active tariff is controlled by the Modbus commands from your energy management system or other Modbus master.

  • When the meter is set to input mode, the active tariff is controlled by the status of the digital inputs.

  • When the meter is set to time of day mode, the active tariff is controlled by the day type, the start and end times, and the start and end dates.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.