NHA2778902-13

Configuring advanced setup parameters using the display

You can configure a subset of advanced parameters using the display.
  1. Navigate to Maint > Setup.
  2. Enter the setup password (default is “0”), then press OK.
  3. Navigate to Meter > Advan.
  4. Move the cursor to point to the parameter you want to modify, then press Edit.
  5. Modify the parameter as required, then press OK.
  6. Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
  7. Press Yes to save your changes.

    Advanced setup parameters available using the display

    Parameter

    Values

    Description

    Label This label identifies the device, e.g., “Power Meter”. You cannot use the display to edit this parameter. Use ION Setup to change the device label.
    Load Timer Setpt (A) 0 - 18 Specifies the minimum average current at the load before the timer starts. The meter begins counting the number of seconds the load timer is on (i.e., whenever the readings are equal to or above this average current threshold.
    Pk I dmd for TDD (A) 0 - 18 Specifies the minimum peak current demand at the load for inclusion in total demand distortion (TDD) calculations. If the load current is below the minimum peak current demand threshold, the meter does not use the readings to calculate TDD. Set this to “0” (zero) if you want the power meter to use the metered peak current demand for this calculation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.