NHA2778902-13

Command mode overview

You can use command mode to send a Modbus command to the device which sets the active tariff.

The active tariff is applied to the measured energy until you send another Modbus command that sets a different tariff.

Search for your meter’s Modbus register list at www.se.com to download the Modbus map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.