NHA2778902-13

I/O Modules

NOTE: Applicable only for PM2230 meter model

This section supplements the optional I/O module installation sheets and provides additional information regarding physical characteristics and capabilities of the I/O module.

The I/O modules are available in the following variants:

  • Single channel analog I/O module

  • Two channel analog I/O module

  • Two channel digital I/O module

  • Two channel digital input and relay output module

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.