NHA2778902-13

Time-of-day mode overview

You can use time-of-day mode to create a tariff schedule that specifies where the meter stores energy or input metered data, based on the time of year (month, day), the type of day (every day, weekend, weekday or a specific day of the week), or time-of-day.

The data collected from the different tariffs can then be used in energy audits or similar costing and budget planning purposes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.