NHA2778902-13

Performing resets using ION Setup

Resets allow you to clear all data of a particular type, such as all energy values or all minimum/maximum values.
  1. Start ION Setup.
  2. Connect to your meter.
  3. Navigate to Meter Resets.
  4. Select a parameter for reset and click Reset.
    The selected parameter value gets cleared.

    Reset parameters

    Option Description
    Meter Initialization Clears all data listed in this table.
    Min/Max Clears all the minimum and maximum registers.
    Active Load Timer Resets all active load timer logs.
    Demands Clears all the demand registers.
    Peak Demands Clears all the peak demand values.
    Energies Clears all accumulated energy values (kWh, kWh1, kWh2, kWh3, kVARh, kVARh1, kVARh2, kVARh3, kVAh, kVAh1, kVAh2, kVAh3), and Run hours.
    Digital Outputs Clears all digital output values.
    Digital Output Counters Clears all the digital output counters.
    Digital Output On Times Clears all the digital output on time logs.
    Status Input Counters Clears all the input counters.
    Status Input On Times Clears all the input on time logs.
    Alarm Counters Clears all the alarm counters and alarm logs.
    Data Log #1 Clears all the data logs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.