NHA2778902-13

Configuring the LED for alarms using the display

You can use the meter display to configure the alarm / energy pulsing LED for alarming.
  1. Navigate to the Maint > Setup > LED.
  2. Set the mode to Alarm, then press OK.
  3. Press the up arrow to exit. Press Yes to save your changes.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.