NHA2778902-13

Pulse output

NOTE: Applicable only for PM2210 meter model

The meter is equipped with one pulse output port (D1+, D1-).

You can configure the pulse outputs for use in the following application:

  • energy pulsing applications, where a receiving device determines energy usage by counting the k_h pulses coming from the meter’s pulse output port.

One pulse output can handle voltage less than or equal to 40 V DC (20 mA maximum). For higher voltage applications, use an external relay in the switching circuit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.