NHA2778902-13

Setting the clock

The Clock setup screens allow you to set the meter’s date and time.
  1. Navigate to Maint > Setup.
  2. Enter the setup password (default is “0”), then press OK.
  3. Navigate to Clock.
  4. Move the cursor to point to the parameter you want to modify, then press Edit.
  5. Modify the parameter as required, then press OK.
  6. Press Yes to save your changes.
  7. Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
  8. Press the up arrow to exit.
  9. Press Yes to save your changes.
    Parameter

    Values

    Description

    Date DD/MM/YY, MM/DD/YY, YY/MM/DD Set the current date using the format displayed on screen, where DD = day, MM = month and YY = year.
    Time HH:MM:SS (24 hour format), HH:MM:SS AM or PM Use the 24-hour format to set the current time in UTC (GMT).
    Meter Time GMT, Local Select GMT to display the current time in UTC (Greenwich Mean Time zone). To display local time, set this parameter to Local, then use GMT Offset (h) to display local time in the proper time zone.

    To configure the clock using ION Setup, see the “PM2000 series meter” topic in the ION Setup online help or in the ION Setup device configuration guide, available for download at www.se.com.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.