NHA2778902-13

Meter resets

Resets allow you to clear various accumulated parameters stored on your meter or reinitialize the meter or meter accessories.
**reset behaviour must be validated with dev for next PM8xxx project

Meter resets clear your meter’s onboard data logs and other related information. Resets are typically performed after you make changes to the meter’s basic setup parameters (such as frequency, VT/PT or CT settings) to clear invalid or obsolete data in preparation for putting the meter into active service.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.