NHA2778902-13

Analog input applications

The analog inputs interpret an incoming analog current signal from transducers. The analog I/O module can measure current using standard 4 - 20 mA analog transducers.

For analog input operation, the meter takes an analog input signal and provides the resulting scaled value. Analog inputs may show a value below zero scale if an open circuit is detected on the input port.

You can set the analog input’s mode for current sensing.

Wiring the analog input

Wiring the dual analog inputs

You can configure the following analog inputs on your meter:

Code

Unit

Description

0

No units

1

%

Percentage

2

ºC

Degrees Celsius

3

ºF

Degrees Fahrenheit

4

Deg

Degrees Angular

5

Hz

Hertz

6

A

Amperes

7

kA

Kilo Amperes

8

V

Volts

9

kV

Kilo Volts

10

MV

Mega Volts

11

W

Watts

12

kW

Kilowatts

13

MW

Megawatts

14

VAR

Volt-Ampere Reactive

15

kVAR

Kilo Volt-Ampere Reactive

16

MVAR

Mega Volt-Ampere Reactive

17

VA

Volt-Amperes

18

kVA

Kilo Volt-Amperes

19

MVA

Mega Volt-Amperes

20

WH

Watt-Hour

21

kWH

Kilowatt-Hour

22

MWH

Megawatt-Hour

23

VARH

Reactive Volt-Ampere Hour

24

kVARH

Reactive Kilo Volt-Ampere Hour

25

MVARH

Reactive Mega Volt-Ampere Hour

26

VAH

Volt-Ampere Hours

27

kVAH

Kilo Volt-Ampere Hours

28

MVAH

Mega Volt-Ampere Hours

29

Seconds

Seconds

30

Minutes

Minutes

31

Hours

Hours

32

Bytes (RAM)

Bytes

33

kBytes (RAM)

Kilobytes

34

$

Dollars

35

gal

Gallons

36

gal/hr

Gallons/hour

37

gal/min

Gallons/minute

38

cfm

Cubic feet/min

39

PSI

PSI

40

BTU

BTU

41

L

Liters

42

ton-hours

Ton-hours

43

l/hr

Liters/hour

44

l/min

Liters/min

45

Euros

46

ms

Milliseconds

47

m3

Cubic-meters

48

m3/sec

Cubic-meters/sec

49

m3/min

Cubic-meters/min

50

m3/hr

Cubic-meters/hour

51

Pa

Pascals

52

Bars

Bar

53

RPM

Revolutions/min

55

BTU/hr

BTU/hour

56

PSIG

Pounds/square inch gauge

57

SCFM

Standard cubic feet/min

58

MCF

Thousand cubic feet

59

Therm

Therm

60

SCFH

Standard cubic feet/hour

61

PSIA

Pounds/square inch absolute

62

lbs

Pounds

63

kg

Kilogram

64

klbs

Kilopounds

65

lb/hr

Pound/hour

66

ton/hr

Ton/hour

67

kg/hr

Kilogram/hour

68

in. Hg

Inch of Mercury

69

kPa

KiloPascals

70

%RH

Percentage of relative humidity

71

MPH

Miles per hour

72

m/sec

Meters/sec

73

mV/cal/(cm²/min)

MilliVolts/calorie/(square centimeters/min)

74

in

Inches

75

mm

Millimeter

76

GWH

GigaWatt-Hour

77

GVARH

Reactive Giga Volt-Ampere Hour

78

GVAH

Giga Volt-Ampere Hours

79

AH

Ampere-Hours

80

kAH

Kiloamp-Hours

81

Therm/hr

Therm/hour

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.