NHA2778902-13

Power quality

The meter provides complete harmonic distortion measurement, recording, and real-time reporting, up to the 15th harmonic for PM2220 and up to 31st harmonic for PM2230 for all voltage and current inputs.

The following power quality measurements are available:

  • PM2220: Individual odd harmonics up to 15th order (Voltage and current, per phase)

  • PM2230: Individual odd harmonics up to 31st order (Voltage and current, per phase)

  • Total harmonic distortion (THD%) for current and voltage (displays line-to-line or line-to-neutral, based on selected system configuration)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.