NHA2778902-13

Alarm log

Alarm records are stored in the meter’s alarm history log.

By default, the meter can log the occurrence of any alarm condition. Each time an alarm occurs it is entered into the alarm log. The alarm log in the meter stores the pickup and dropout points of alarms along with the date and time associated with these alarms. You can view and save the alarm log to disk, and reset the alarm log to clear the data out of the meter’s memory.

The meter stores alarm log data in non-volatile memory. The size of the alarm log is fixed at 40 records.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.