NHA2778902-13

Resetting alarms using ION Setup

Use ION Setup to reset alarms.

You can also reset alarms using the meter display.

  1. Connect to your meter in ION Setup.
  2. Open the Meter Resets screen.
  3. Select the alarm parameters to clear and click Reset.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.