NHA2778902-13

Setting the rate

The Rate setup screens allow you to set the different rate parameters.
  1. Navigate to Maint > Setup.
  2. Enter the setup password (default is “0”), then press OK.
  3. Navigate to Rate.
  4. Move the cursor to point to Rate1 or Rate2 to modify, then press Edit.
  5. Move the cursor to point to Channel or Factor per (k__h) to modify, then press Edit.
  6. Modify the parameter as required, then press OK.
  7. Press up arrow and press Yes to save your changes.
  8. Press the up arrow to exit.
    Parameter

    Values

    Description

    Label

    Rate1 / Rate2

    Example: CO2 Emission, Energy Cost

    You can edit the label using ION Setup
    Channel None, Active Del, Active Rec, Active Del + Rec, Reactive Del, Reactive Rec, Reactive Del + Rec, Apparent Del, Apparent Rec, Apparent Del + Rec Select a channel from the list.
    Factor per (k__h) 0.000 to 99999.999 You can edit the factor value between 0.000 to 99999.999.

    To configure the Rate using ION Setup, see the “PM2000 series meter” topic in the ION Setup online help or in the ION Setup device configuration guide, available for download at www.se.com.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.