NHA2778902-13

Multi-tariff implementation

The meter supports configuration of up to 4 different tariffs to measure and monitor energy usage that can be used in billing or cost applications.

There are three different tariff modes you can use to activate the multi-tariff registers:

  • Command mode

  • Time of Day mode

  • Input mode

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.