NHA2778902-13

Saving the data log contents using ION Setup

You can use ION Setup to save the contents of the data log.
  1. Start ION Setup and open your meter in data screens mode (View > Data Screens. See the ION Setup help for instructions.
  2. Double-click Data Log #1 to retrieve the records.
  3. Once the records have finished uploading, right-click anywhere in the viewer and select Export CSV from the popup menu to export the entire log.
    NOTE: To export only selected records in the log, click the first record you want to export, hold down the SHIFT key and click the last record you want to export, then select Export CSV from the popup menu.
  4. Navigate to the folder where you want to save the data log file, then click Save.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.