NHA2778902-13

Analog output applications

The analog I/O module can send low current for standard 4 - 20 mA analog transducers.

For analog output operation, the meter takes an input value and scales it to the appropriate signal value to send out the physical analog output port.

Wiring the analog output

Wiring the dual analog output

You can configure the following analog outputs on your meter:

Parameters

Description

Current

Current: Phase wise

Current Average

Current Unbalance: Phase wise

Current Unbalance Worst

Voltage

Voltage L-L: Phase wise

Voltage L-L Avg

Voltage L-N: Phase wise

Voltage L-N Avg

Voltage Unbalance L-L: Phase wise

Voltage Unbalance L-L Worst

Voltage Unbalance L-N: Phase wise

Voltage Unbalance L-N Worst

Power

Active Power: Phase wise

Active Power Total

Reactive Power: Phase wise

Reactive Power Total

Apparent Power: phase wise

Apparent Power Total

PF

PF Total

Frequency

Frequency

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.