NHA2778902-13

Logs overview

This chapter briefly describes the following logs of the meter:

  • Alarm log

  • User-defined data log

Logs are files stored in the non-volatile memory of the meter and are referred to as “on-board logs”.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.