NHA2778902-13

SnapShot setting

  1. Navigate to Maint > Setup.
  2. Enter the setup password (default is “0”), then press OK.
  3. Navigate to Snap.
  4. Press Snap. The SnapShot screen appears.
  5. Press Edit to select the SnapShot time in HH:MM.
  6. Press + to increment the active digit through the numerals 0-9.
  7. Press ◄ to enter the selected character and move to the character on the left.
  8. Continue until all values are selected, then press OK to set the time.
    • Press Yes to accept the changes and return to the previous screen.

    • Press No to keep the existing configuration and return to the previous screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.