DOCA0170EN-06

Test Report

Perform the following steps to generate automatic trip test report:

  1. Click Reports > Project Report.
    The generated project report is displayed in a new tab.
  2. Save or print the project report as required.

    The project report is a confirmation of accurate protection settings of the circuit breaker.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?