DOCA0170EN-06

EcoStruxure Power Commission Software

Overview

EcoStruxure Power Commission (EPC) software helps you to manage a project as part of testing, commissioning, and maintenance phases of the project life cycle. The innovative features in it provide simple ways to configure, test, and commission the smart electrical devices.

EPC software automatically discovers the smart devices and allows you to add the devices for an easy configuration. You can generate comprehensive reports as part of Factory Acceptance Test and Site Acceptance Test to replace your heavy manual work. Additionally, when the panels are under operation, any change of settings made can be easily identified by a yellow highlighter. This indicates the difference between the project and device values, and hence provides a system consistency during the operation and maintenance phase.

For more information, refer to the EcoStruxure Power Commission Online Help.

Click here to download the latest version of EcoStruxure Power Commission.

Features

EPC software performs the following actions through Service Interface:

  • Create projects by device discovery.

  • Save the project in the EPC cloud for reference.

  • Download the protection settings from the device.

  • Perform test operation in a secured way.

  • View the communication architecture between the devices in graphical representation.

  • Check system firmware compatibility status.

  • Update to the latest device firmware.

  • Perform automatic trip curve, Zone-Selective Interlocking (ZSI) tests, force trip tests, and prepare for primary injection tests.

  • Generate and print test reports.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.