DOCA0170EN-06

Test Functions

EPC allows you to perform the following tests on non-communicating MicroLogic trip units through the Service Interface:

  • Automatic trip curve test using secondary injection

  • Device check up (Forced trip test)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.