DOCA0170EN-06

Connection of the Service Interface to an Enerlin'X Device

Use the cable LV485514SP to connect the Service Interface to one of the RJ45 ULP ports of the following Enerlin'X devices:

  • IFM interface

  • IFE interface

  • IFE server

  • IO module

  • FDM121 display

  1. AC/DC power

  2. ULP cable

  3. USB cable with magnet

After connected, you can use EcoStruxure Power Commission software to configure and/or update the firmware of:

  • The Enerlin'X device on which the Service Interface is connected.

  • The other Enerlin'X devices in the IMU, including the BCM ULP.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.