DOCA0170EN-06

Automatic Trip Curve Tests with Custom Test Points

It is recommended that you follow the guidelines while defining the custom test points:

  • Decimal values for the injection current are considered as invalid inputs.

  • The selected protection trip type must match the test segment of the time-current curve. If an incorrect value is selected, the test results may be misleading. For example:

    • If you select the short-time protection trip type and enter the injection current value within the short-time current range, then the MicroLogic trip unit trips in short-time segment. This indicates a Passed test status.

    • If you select the short-time protection trip type and enter the injection current value within the long-time current range, then the MicroLogic trip unit trips in long-time segment.

      The test results do not display the cause of the trip. Because the circuit breaker has tripped, the test results indicate a Passed test status.

    • If you want to test the ground fault protection but select any protection type that inhibits ground fault protection, then the test results are incorrect.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.