DOCA0170EN-06

Hardware Description

Service Interface Description

  1. 24 Vdc power input

  2. 24 Vdc power output

  3. Mini-B USB port

  4. Test port LED

  5. Status LED

  6. USB LED

  7. QR code to product information

  8. Power LED

  9. Magnetic Service Interface holder

  10. Test port

  11. Rubber protective cover

  12. Magnetic cable holder

Accessories Part Numbers

The Service Interface is delivered with the following accessories:

Accessories

Description

Part number

AC/DC power

LV485511SP

7-pin cable for 630–6300 A ACB MCCB trip units

LV485512SP

7-pin cable for 100–630 A MCCB trip units

LV485513SP

ULP cable

LV485514SP

USB cable with magnet

LV485517SP

24 Vdc power output connector

Dinkle - EC350V–02P

Phoenix Contact - 1840366

Power Supply

The Service Interface is supplied with 24 Vdc through the 24 V power adapter port. 110...230 Vac to 24 Vdc adapter is supplied with Service Interface along with adapter plugs for Europe (RPE), UK (RPK), USA (RPA), and Australia (RPS). The plugs are 2-pin type.

The Service Interface is also fitted with a 24 Vdc at 120 mA output to power any auxiliary devices, if necessary.

Test Port LED

The test port LED indicates the connection status of the Service Interface.

LED indication

LED color

Status description

@Updated D1

ON

Green

Successful connection between Service Interface and MicroLogic trip unit mounted in the following circuit breakers with a cable LV485512SP.

  • MasterPacT NT/NW

  • EasyPacT MVS

  • ComPacT NS

  • PowerPacT P- and R-frame

Blue

Successful connection between Service Interface and MicroLogic trip unit mounted in the following circuit breakers with a cable LV485513SP.

  • ComPacT NSX

  • PowerPacT H-, J-, or L-frame

@Updated D2

FLASH (every 1 s)

Orange

Successful connection between Service Interface and Enerlin'X device with a cable LV485514SP.

@Added D1

FLASH (every 2 s)

Green

Unsuccessful connection between Service Interface and MicroLogic trip unit mounted in the following circuit breakers with a cable LV485512SP.

  • MasterPacT NT/NW

  • EasyPacT MVS

  • ComPacT NS

  • PowerPacT P- and R-frame

The possible reasons for unsuccessful connection are:

  • The cable is inoperative.

  • The cable is not properly connected to the trip unit.

  • The communication between the Service Interface and trip unit is unstable.

Blue

Unsuccessful connection between:

  • Service Interface and MicroLogic trip unit mounted in the following circuit breakers with a cable LV485513SP.

    • ComPacT NSX

    • PowerPacT H-, J-, or L-frame
  • Service Interface and Enerlin'X device with a cable LV485514SP

    .

The possible reasons for unsuccessful connection are:

  • The cable is inoperative.

  • The cable is not properly connected to the trip unit.

  • The communication between the Service Interface and trip unit or an Enerlin'X device is unstable.

OFF

Service Interface is not connected to a trip unit.

Power LED

The green power LED indicates the power supply status.

LED indication

Status description

ON

Power input connected

OFF

Power input not connected

USB LED

The green USB LED indicates the USB connection status.

LED indication

Status description

ON

USB connected

OFF

No USB connected

Status LED

The orange status LED indicates the Service Interface status.

LED indication

Status description

ON

Service Interface in Boot mode

OFF

Service Interface operational

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.