DOCA0170EN-06

Firmware Update

Description

Use the latest version of EcoStruxure Power Commission software for all firmware updates.

The latest version of Service Interface firmware is updated in a single operation through EcoStruxure Power Commission software.

For more information about Service Interface firmware versions, refer to Service Interface - Firmware Release Notes.

Signed Firmware

All firmware designed for the IMU with a MasterPacT NT/NW, EasyPacT MVS, ComPacT NS, PowerPacT P- and R-frame, ComPacT NSX, or PowerPacT H-, J-, or L-frame circuit breaker is signed using the Schneider Electric public key infrastructure.

The digital certificates used to authenticate genuine Schneider Electric firmware and software must be regularly verified to ensure that they are still valid. Digital certificates that are no longer valid are published on the Certificate Revocation List (CRL) available on the Schneider Electric Cybersecurity Support Portal.

For more information on cybersecurity for the MasterPacT MTZ circuit breakers, refer to MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide.

Updating the Firmware Version

To update the Service Interface firmware with EcoStruxure Power Commission software:

  1. Select Connect to device directly on the home screen.

  2. Check the Service Interface firmware version in Analyze Firmware Status.

  3. If the recommended action is to update the firmware, select the check box next to Service Interface then click Next.

  4. Click Upgrade.

  5. Enter the Service Interface password in the dialog box and click CONTINUE.

    Firmware update begins. A green icon with a tick displays when firmware update is completed.

    IMPORTANT: Do not disconnect the Service Interface until the firmware update is complete.
  6. Click the arrow next to Module upgraded to display the current and latest Service Interface firmware versions.

  7. Close the Analyze Firmware Status window.

For more information, refer to the EcoStruxure Power Commission Online Help.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.