DOCA0170EN-06

Discovering Trip Units

After the PC is connected to the MicroLogic trip unit to test using the Service Interface, you can start the EPC.

Perform the following steps to discover the devices:

  1. Click Launch Device Discovery.
    The Add devices window is displayed.
  2. Click USB/SERIAL from Find devices via.
  3. Select the device to test or click FIND DEVICES.
  4. Select the device to test from the Device List and click ADD DEVICES.
    The Project details dialog box is displayed.
  5. Enter project and customer details and then click NEXT.
    The Device view page is displayed.
  6. Click CONNECT TO DEVICE.

    The following buttons for the selected device are displayed:

    • Configure

    • Device Check up

    • Firmware

    • Automatic Trip Curve Test

    • Zone-Selective Interlocking Test

    • Prepare for Primary Injection Test

    For more information, refer to the EcoStruxure Power Commission Online Help.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.