DOCA0170EN-06

Introduction

PacT Series Master Range

Future-proof your installation with Schneider Electric’s low-voltage and medium-voltage PacT Series. Built on legendary Schneider Electric innovation, the PacT Series comprises world-class circuit breakers, switches, residual current devices and fuses, for all standard and specific applications. Experience robust performance with PacT Series within the EcoStruxure-ready switchgear, from 16 to 6300 A in low-voltage and up to 40.5 kV in medium-voltage.

Overview

The Service Interface with part number LV485500 is a portable instrument for field testing.

The Service Interface is used:

  • For configuration of Enerlin'X devices.

  • For testing and configuration of MicroLogic trip units mounted in the following low voltage circuit breakers:

    • MasterPacT™ NT/NW circuit breakers

    • EasyPacT™ MVS circuit breakers

    • ComPacT™ NS circuit breakers

    • PowerPacT P- and R- frame circuit breakers

    • ComPacT™ NSX circuit breakers

    • PowerPacT H-, J-, and L-frame circuit breakers

NOTE:
  • The information related to the new generation of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers in this guide applies to the existing range ComPact NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.

  • The information related to the new generation of ComPacT NS and PowerPacT P- and R-frame circuit breakers in this guide applies to the existing range ComPact NS and PowerPact P- and R-frame circuit breakers also. The exceptions are mentioned wherever applicable.

  • These new ranges are based on the same technical and dimensional architecture as that of the existing range of circuit breakers.

EcoStruxure Power Commission (EPC) software is used for testing the circuit breakers and communication accessories through the Service Interface.

Features

The main features of Service Interface are:

  • Single connector interface for testing different circuit breakers.

  • 24 Vdc at 120 mA power output for external devices.

  • 12 kV safety impulse protection between user interface and test port.

  • Magnet mountable.

  • EPC user interface for test and configuration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.