DOCA0170EN-06

Test Report

  1. Click Reports > Project Report.

    The generated project report is displayed in a new tab.

  2. Save or print the project report as required.

    The project report is the confirmation of correct mechanical operation trip of the circuit breaker.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.