DOCA0170EN-06

Test Functions

EPC software allows you to:

  • Perform the following tests on communicating MicroLogic trip unit through the Service Interface.

    • Automatic trip curve test using secondary injection

    • Device check up (Force trip test)

    • ZSI test

  • Prepare primary injection tests on communicating MicroLogic trip unit through the Service Interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.