DOCA0170EN-06

Test Report

  1. Click Reports > Project Report.

    The generated project report is displayed in a new tab.

  2. Save or print the project report as required.

The project report is a confirmation that the ZSI test verifies field wiring between multiple circuit breakers connected in a ZSI system.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.