DOCA0170EN-06

Test Procedure

Perform the following steps for the force trip test:

  1. Click Device Check up in the Device view page.
  2. Click the Device tab.
  3. Close the circuit breaker or verify that the circuit breaker is closed.
  4. Click FORCE TRIP.
    The DANGER safety message is displayed.
    DANGER
    hazard of electrical shock, explosion or arc flash
    Do not continue with this operation without confirming that doing so will not create a hazardous situation.
    Failure to follow these instructions will result in death or serious injury.
  5. Read the DANGER safety message, and if understood, click I UNDERSTAND.
  6. Enter the MicroLogic Administrator password in the dialog box and click CONTINUE.
  7. Verify that the circuit breaker is tripped.
    The Force Trip Result Table displays the force trip status as successful.
    NOTE: Click REPEAT, if required.

    The test procedure is repeated from step 4.

    The WARNING safety message is displayed.

    WARNING
    Hazard of executing injection test
    Make sure to reset and close the circuit breaker before executing an injection test.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  8. Click CANCEL to close the Force Trip Result Table dialog box.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.