DOCA0170EN-06

Connection of the Service Interface to a MicroLogic Trip Unit

Connect the Service Interface to the MicroLogic trip unit test port using the cable LV485513SP.

  1. AC/DC power

  2. 7-pin cable for 100-630 A MCCB trip units

  3. USB cable with magnet

IMPORTANT: It is recommended to supply the MicroLogic 5/6/7 trip unit with a 24 Vdc external power supply during the tests to reduce the test duration.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?