DOCA0170EN-06

Configuration Function

You can configure the MicroLogic A, E, P, and H trip units with the Service Interface from EPCwhen the PC is connected to the MicroLogic trip unit.

@Updated D2
You can save the configurations of MicroLogic A, E, P, and H trip units in the EPC.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?