Test Procedure
Perform the following steps for automatic trip curve test:
- Click Automatic Trip Curve Test in the Device view page.
- Select Preconfigured test point or Custom test point and click RUN TEST.The NOTICE message is displayed.NOTICE HAZARD OF LOSS OF POWER- During these tests, the circuit breaker will trip, resulting in loss of power to downstream devices.
- It is recommended to perform these tests in conjunction with proper planning, precautions, and per the test schedules.
 Failure to follow these instructions can result in disruption due to loss of power.For Preconfigured test point, to run a different protection test to generate a report, refer to Automatic Trip Curve Tests with Preconfigured Test Points. 
- Read the NOTICE message, and if
                  understood, click I UNDERSTAND.The Password Required dialog box is displayed.
- Enter the MicroLogic Administrator password in the dialog box and click CONTINUE.
- Reset and open the circuit breaker.
-  Click OK.The protection test starts.NOTE: During the long-time protection test:- 
                           Injection Time and Remaining Time before trip (in seconds) are displayed. 
- 
                           You can click ABORT to stop the running test. This cancels all the subsequent tests. 
 NOTE: The short-time protection cannot be tested if Ir x Isd > Ii.
- 
                           
- Repeat step 5 and 6 for the next test.