DOCA0170EN-06

Discovering Trip Units

After the PC is connected to the non-communicating MicroLogic trip unit to test through the Service Interface, you can start the EPC.

Perform the following steps to discover the devices:

  1. Click Launch Device Discovery.

    The Add devices window is displayed.

  2. Click USB/SERIAL from Find devices via option button.
  3. Select the device to test or click FIND DEVICES.
  4. Select the COM port of Service Interface from the list and click ADD DEVICES.

    The Add device details dialog box is displayed.

  5. Enter device details and click SAVE.
  6. Enter project and customer details and then click CONTINUE.

    The Device view page is displayed.

  7. Click CONNECT TO DEVICE.

    The following buttons for the selected device are displayed:

    • Configure

    • Device Check up

    • Firmware

    • Automatic Trip Curve Test

    For non-communicating trip units, Configure and Firmware buttons are displayed but not available. Configuration and firmware update are not supported in non-communicating trip units.

    For more information, refer to the EcoStruxure Power Commission Online Help.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.