DOCA0170EN-06

Enerlin'X Device Compatibility

The following table lists which functions are applicable for Enerlin'X devices with the Service Interface connected to PC with EPC software:

Device

Part number

Configuration

Firmware update

IO input/output application module for one circuit breaker

LV434063

FDM121 front display module for one circuit breaker

TRV00121

STRV00121

IFE Ethernet interface for one circuit breaker

LV434001

IFE switchboard server

LV434002

IFM Modbus-SL interface for one circuit breaker with Modbus-SL RJ45 port

LV434000

IFM Modbus-SL interface for one circuit breaker with Modbus-SL 5-pin connector

TRV00210

STRV00210

BSCM circuit breaker status control module

LV434205

S434205

BCM ULP circuit breaker communication module

33106

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.