DOCA0170EN-06

Configuration Function

You can configure the MicroLogic 5, 6, and 7 trip units with the Service Interface from EPC software when the PC is connected to the MicroLogic trip unit.

The settings of MicroLogic 5, 6, and 7 trip units can be saved by using EPC software.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.