DOCA0170EN-06

Test Functions

EPC software allows you to perform the following tests on MicroLogic trip unit through the Service Interface:

  • Automatic Trip Curve test using secondary injection

  • Device check up (Force trip test)

  • ZSI test

EPC software also allows you to prepare primary injection tests on MicroLogic trip unit through the Service Interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.