Test Procedure
Perform the following steps for the automatic trip curve test:
- Click Automatic Trip Curve Test in the Device view page.
- Select Preconfigured test point or Custom test point and click RUN TEST.
- Enter the protection settings details and click SAVE.The NOTICE message is displayed.NOTICE HAZARD OF LOSS OF POWER- During these tests, the circuit breaker will trip, resulting in loss of power to downstream devices.
- It is recommended to perform these tests in conjunction with proper planning, precautions, and per the test schedules.
 Failure to follow these instructions can result in disruption due to loss of power.
- Read the NOTICE message, and if
                  understood, click I UNDERSTAND.The Password Required dialog box is displayed.
- Enter the MicroLogic Administrator password in the dialog box and click CONTINUE.
- Reset and close the circuit breaker.
- Click OK.The protection test starts.NOTE: During the long-time protection test:- 
                           Injection Time and Remaining Time before trip (in seconds) are displayed. 
- 
                           You can click ABORT to stop the running test. This cancels all the subsequent tests. 
 NOTE: The short-time protection cannot be tested if Ir x Isd > Ii.
- 
                           
- Repeat step 6 and 7 for the next test.The test result is displayed at the end of the test. After completing all the tests, the Test Results screen is displayed with:- 
                        The list of protection functions tested. 
- 
                        The injection current. 
- 
                        The protection settings. 
- 
                        The expected trip time and the real trip time. 
- 
                        The test result. 
 NOTE: For non-communicating trip units, the Service Interface cannot reset thermal memory. Therefore, 15 minutes time period must be observed between long time tests.
-