MicroLogic Trip Unit Compatibility
The following table indicates which functions are applicable for MicroLogic trip units:
|
MicroLogic trip units |
Configuration |
Alarm simulation |
Firmware update |
Automatic trip curve test using secondary injection |
Force trip test |
ZSI test |
Preparation for primary injection tests |
||
|---|---|---|---|---|---|---|---|---|---|
|
Inhibit thermal memory |
Inhibit ground fault |
||||||||
|
With pre-configured test points |
With custom test points |
||||||||
|
MicroLogic 1.2, 1.3, 2.2, 2.3, 3.2, 3.3, |
– |
– |
– |
✓ |
✓ |
✓ |
– |
✓ |
– |
|
MicroLogic 5.2 B, 5.3 B |
✓ |
– |
– |
✓ |
✓ |
✓ |
– |
✓ |
– |
|
MicroLogic 5.2 A/E, 5.3 A/E |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
– |
|
MicroLogic 6.2 A/E, 6.3 A/E |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
|
MicroLogic |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
✓ |
– |
These MicroLogic trip units can be mounted in the following circuit breakers:
-
ComPacT NSX circuit breakers
-
PowerPacT H-, J-, and L-frame circuit breakers