DOCA0170EN-06

Connection of the Service Interface to a MicroLogic Trip Unit

Connect the Service Interface to the MicroLogic trip unit test port using the cable LV485512SP.

  1. AC/DC power

  2. 7-pin cable for 630–6300 A ACB MCCB trip units

  3. USB cable with magnet

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.