Test Procedure
- Click Device Check up in the Device view page.
- Click the Device tab.
- Close the circuit breaker or verify that the circuit breaker is closed.
- Click FORCE TRIP.
The DANGER safety message is displayed.
DANGERhazard of electrical shock, explosion or arc flashDo not continue with this operation without confirming that doing so will not create a hazardous situation.Failure to follow these instructions will result in death or serious injury. - Read the DANGER safety message, and if understood, click I UNDERSTAND.
- Enter the MicroLogic Administrator password in the dialog box and click CONTINUE.
- Verify that the circuit breaker is physically tripped.The Force Trip Result Table displays the force trip status as successful.
NOTE: Click REPEAT, if required.The test procedure is repeated from step 4.
The WARNING safety message is displayed.
WARNINGHazard of executing injection testMake sure to reset and close the circuit breaker before executing an injection test.Failure to follow these instructions can result in death, serious injury, or equipment damage. - Click CANCEL to close the Force Trip Result Table dialog box.