DOCA0193EN-00

IFM Interface

Overview

The IFM Modbus-SL interface for one circuit breaker enables an intelligent modular unit with an EasyPact MVS circuit breaker, to be connected to a two-wire Modbus-SL RS-485 serial line Modbus network. Each circuit breaker has its own IFM interface and a corresponding Modbus address.

The part number of the IFM interface is LV434000.

Features

The main features of IFM interface are:

  • Single Modbus serial line interface provided in

    • RJ45 connector interface

    • Stacking connection interface

  • Rotary switches for address settings and padlock option

  • Pushbutton for test functionality

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.